12/10/2024 1:45 PM | |
Joined: 7/11/2022 Last visit: 8/25/2025 Posts: 56 Rating:
|
Hi, I believe this needs to be published in the WinCC Unified Systems. Additionally, please take a look at this forum post. |
12/11/2024 3:14 AM | |
Joined: 8/6/2024 Last visit: 9/12/2025 Posts: 24 Rating:
|
Screen.Items("Trend control_1").FireCommand(10,true); I think you can use custom ID,I test code,it is OK! |
12/11/2024 8:39 AM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4107 Rating:
|
Hi,
According to the readme, with V18 the ExecuteToolbarButton system function is only available for system diagnostics control, parameter set control and alarm control. Kind regards |
12/13/2024 9:41 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Yes I would also say in V18 this is not yet supported. you would need TIA V19 or newer. Here there are also the mentioned Systemfunction for the trend control available and also the Start/Stop. The Firecommand in V17/18 was not supported for every control... Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on