7/29/2013 3:06 PM | |
Posts: 767 Rating:
|
Hello innovations, Your decision of which compact flash card is required depends upon on how many axes are controlled by the CU320-2 multi axis controller. If three (3) or fewer axes are controlled by the CU320-2 multi axis controller then the Compact Flash without performance expansion is sufficient. 6SL3054-0EE00-1BA0 SINAMICS S120 COMPACTFLASH CARD W/O PERFORMANCE EXTENSION INCLUDING CERTIFICATE OF LICENCE V4.04 If four (4) more axes are controlled by the CU320-2 multi axis controller then the Compact Flash with performance expansion is required. 6SL3054-0EE01-1BA0 SINAMICS S120 COMPACTFLASH CARD WITH FIRMWARE OPTION PERFORMANCE-EXTENSION INCLUDING CERTIFICATE OF LICENCE V4.4 Best Regards, Deputy AttachmentCompact Flash.pdf (1021 Downloads) |
Last edited by: O_Moderator at: 7/30/2013 8:35 AMattachment reattached Last edited by: Deputy at: 7/29/2013 3:07 PM |
|
7/29/2013 3:18 PM | |
Posts: 767 Rating:
|
Hello Innovations, If you are building a drive system which is new then you should likely choose the most current compact flash card, which would be one of the folllowing which is a larger 2 GB compact flash card. 6SL3054-0EG00-1BA0 SINAMICS S120 COMPACTFLASH CARD W/O PERFORMANCE EXTENSION INCLUDING CERTIFICATE OF LICENCE V4.06 6SL3054-0EG01-1BA0 SINAMICS S120 COMPACTFLASH CARD WITH FIRMWARE OPTION PERFORMANCE-EXTENSION INCLUDING CERTIFICATE OF LICENCE V4.06 Below link is for documentation of version 4.6 firmware and description of benefits of the larger capacity compact flash card. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=67385242&nodeid0=10803928&nodeid5=38718979&onlyConfigurable=on&load=content&csQuery0=6SL3054%2D0EG00%2D1BA0&subtype=130000&lang=en&extranet=standard&viewreg=WW&u=NDAwMDAxNwAA&siteID=cseus Best Regards, Deputy |
7/29/2013 4:24 PM | |
Joined: 5/21/2008 Last visit: 5/31/2025 Posts: 93 Rating:
|
Dear Deputy, thanks a lot for the support, you cleared my doubts over it. regards |
Follow us on