12/16/2024 12:58 PM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi and.short, Regarding this question, Unified Comfort Panel (UCP) panels are computers with a Linex operating system based on Debian: Debian 10 (V17) or Debian 11 (V18) Debian 12 (V19). On the other hand, I would like to point out that access to the operating system is not free. Access to the operating system is protected, any attempt to interfere with the operating system may affect its functionality. Therefore, I recommend that you do not make any modifications so as not to harm this equipment. Best regards! |
If this Information really helps, you could use the Rate function |
|
12/16/2024 1:55 PM | |
Joined: 3/19/2017 Last visit: 6/18/2025 Posts: 21 Rating:
|
@Stefan Arcularius, Many thanks for your quick reply. In response to ElonksuM_SN_BN, siemens provides a way to install docker apps on the panel (through what it calls Edge App Publisher). No hacking required. Have a look at the following link: |
Last edited by: and.short at: 12/16/2024 13:56:14Last edited by: Moderator_Lan at: 12/16/2024 14:13:47link optimized |
|
This contribution was helpful to
1 thankful Users |
Follow us on