2/19/2025 4:32 PM | |
Joined: 2/17/2020 Last visit: 8/29/2025 Posts: 1251 Rating:
|
Hi, The first thing I would check would be whether deleting the DCF file from the WinCC project improves the situation, as sometimes an inconsistent DCF file can cause a slow start Runtime: Update the configuration file of the WinCC project (delete DCF) If this only happens with the project's Autostart, then please check the FAQ below: How do you avoid synchronization problems with the Autostart of WinCC Runtime V7? |
A rating will be well appreciated. |
|
2/21/2025 11:20 AM | |
Joined: 8/3/2009 Last visit: 9/8/2025 Posts: 16353 Rating:
|
Hello AutoGen_955623 It could also be that there are blocked SQL Server connections still in SQL Server that have a negative effect on the performance: you can have a look in the Management Studio if it is so: https://support.industry.siemens.com/cs/de/en/view/109818900 Also you should not use a tool large archive configuration and too many single segments. If you give us an example with WinCC Version and which Archive Configuration you use we could probably tell more about it Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on