5/31/2012 4:26 AM | |
Posts: 12 Rating:
|
Dear Technical, I am new with this modbus open tcp communication. I downloaded the working program on this site to communicate with compressor via modbus tcp. There are 3 compressor to communicate with, I am using CPU 315-2pn/dp.. Here i attached the program i am working with, no data coming from compressor on designated db's.. Thanks in advance... Regards, Heartbroken AttachmentModbus_tcp.zip (521 Downloads) |
5/31/2012 11:22 AM | |
Posts: 3093 Rating:
|
Hello Hearbroken, I used this example (FB10)before and I recognized that it doesn't work properly. I recommend to use the Simatic AddOnModbusTCP for PN CPUs, Regards, Kaulquappe |
5/31/2012 3:53 PM | |
Posts: 12 Rating:
|
Kaulquappe, Part 1 of ad-0ns open modbus tcp.. see attcahed file. thanks in advance, heartbroken
AttachmentTest_modbus.part1.zip (505 Downloads) |
5/31/2012 4:00 PM | |
Posts: 12 Rating:
|
Kaulquappe, Part 2 of ad-0ns open modbus tcp.. see attcahed file. thanks in advance, heartbroken
AttachmentTest_modbus.part2.zip (563 Downloads) |
5/31/2012 4:03 PM | |
Posts: 12 Rating:
|
Kaulquappe, Part 3 of ad-0ns open modbus tcp.. see attcahed file. thanks in advance, heartbroken
AttachmentTest_modbus.part3.zip (511 Downloads) |
5/31/2012 4:08 PM | |
Posts: 12 Rating:
|
Kaulquappe, Part 4 of ad-0ns open modbus tcp.. see attcahed file. i also create a udt for vilter data arrangement, open modbus tcp is already licensed. thanks in advance, heartbroken
AttachmentTest_modbus.part4.zip (542 Downloads) |
6/1/2012 12:51 PM | |
Posts: 12 Rating:
|
See attached file, print screens of DB's, Vat, OB's of my simatic program. Vilter IP address 192.168.1.50 ID # = 1,192.168.1.60 ID # = 2,192.168.1.70 ID # = 3, all are in master mode.. Now i am working on one vilter(192.168.1.50 ID # = 1). No data has been receive., Open modbus TCP is already licensed. Thanks, heartbroken
AttachmentModbus_print.zip (519 Downloads) |
6/1/2012 1:42 PM | |
Posts: 3093 Rating:
|
Hello Heartbroken, you receive error 809B from TCON (see DB1 DBW88 to DBW98). Online help: "809BThe local_device_id in the connection description does not match the CPU." You didn't parameterize the connection with the wizard. You can download the wizard here Regards, Kaulquappe |
Follow us on