8/15/2019 6:21 AM | |
Joined: 3/31/2018 Last visit: 6/28/2025 Posts: 36 Rating:
|
Hello everyone again, Here what I found: https://mall.industry.siemens.com/mall/en/WW/Catalog/Products/5000038#Overview "In order to avoid errors when replacing modules, the front connector is coded mechanically when first plugged in. Then, it only fits in to the modules of the same type. This avoids, for example, an AC 230 V input signal accidentally being plugged into the DC 24 V module." So when I have replaced module from DI16/DO16 to DO 32, I must have make reset on connector? Does anyone knows how to do that or where this key is located? Regards, Nursultan Nurzhanuly |
Last edited by: Nursultan Nurzhanuly at: 08/15/2019 06:23:52Last edited by: Nursultan Nurzhanuly at: 08/15/2019 11:40:58 |
|
Follow us on