11/27/2019 8:53 AM | |
Joined: 9/9/2014 Last visit: 2/12/2025 Posts: 246 Rating:
|
Hello, If you really need manuals for your module, then they are lower (you can just use the search on our site): SIMATIC S7-300 FM 350-2 Counter Module FM 350-2 Brief Instructions on commissioning FAQ: How do you interconnect an FM350-2 in PCS 7? How do you cyclically read out the 8 channels of the FM 350-2 counter module as quickly as possible? How do you commission the counter module FM 350-2 (6ES7350-2AH01-0AE0) in STEP 7 (TIA Portal)? Which function modules (FM) can be used remotely in an ET 200M? Why does the counter value always jump between 0 and 1 when using a 24-volt encoder? The manual describes in detail how to connect to the module. About the sensor: If it is a PNP or NPN - it doesn't matter, in fact.Type of contact plays a important role - normally closed or normally open (for your case it should be normally open) In your case, you will have a connection (most likely) between the black and blue wires sensor - that is, between the "signal" and the "minus" 24 volts for sensors connections, valid for your module. And if your sensor allows this, then you will take the signal between the black and blue wires - connect it like that |
Last edited by: Jen_Moderator at: 11/27/2019 12:34:39Optimized all links. Best Regards |
|
11/27/2019 11:33 AM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating:
|
Full Project is attached as well : FM-350-2/1 S7 v5.5 Best Regards Soble AttachmentSpeedTes.zip (389 Downloads) |
Website: |
|
This contribution was helpful to
1 thankful Users |
11/28/2019 3:56 PM | |
Joined: 8/3/2017 Last visit: 3/27/2025 Posts: 142 Rating:
|
Thanks everyone for the tips, I´ll try to make it work, and post afterwards! |
11/29/2019 7:26 AM | |
Joined: 9/9/2014 Last visit: 2/12/2025 Posts: 246 Rating:
|
Hello fsgonzaga If our answers somehow helped you, and you solved your question, please close the topic, and put a rating. Thanks! |
Best Regards |
|
Follow us on