12/4/2018 12:10 PM | |
Posts: 44 Rating:
|
Hello There is a problem related to communication between PC & PLC . I have cpu series S7-200 smart and I use Micro-win smart 2.3 According to attached file , I've tried to find the cpu with possible ' transmition rates ' .but I couldn't .I was careful transmission rate is "SET PG/PC Interface and also Microwin software " . So I tried by 9.6, 19.2 and 187.5 kbps but nothing happened and I always revived a massage that is in video in attached file . What is the problem ? Thanks . AttachmentS7-200.zip (698 Downloads) |
Last edited by: hossein82 at: 12/4/2018 12:11:59 PM |
|
12/5/2018 5:53 AM | |
Posts: 44 Rating:
|
Hello Also I checked with Siemens PC Adapter (PPI) according attached picture ,but still I have same problem . With the PC adapter , the main problem is on the software , where I should choose the Interface , I just have 3 options that does not include the PC Adapter and it is while the PC adapter is recognized by windows and it's driver installed correctly..(attached picture.) I tried with the PC adapter to connect Simatic manager and S7-300 and it worked . But for S7-200 Smart and MicroWin 2.3 Smart , it doesn't. Another points that may help to find problem is , I tried MicroWIN.V4.0.SP6 and not Smart CPU (216-2bd23-0xb8) by the PC adapter (PPI), The result was OK and software find the CPU . Does the S7-200 Smart series work only by special interface ?! Thanks AttachmentPictures.zip (604 Downloads) |
12/5/2018 11:41 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, from documentation (hope I'm not wrong) is clear that all Smart CPUs also support one Ethernet port so I don't see problem to try this interface than bother now with serial link. Update: (link) -> Smart PLC Check page 9... |
Last edited by: Duris_I at: 12/5/2018 11:44:34 AMWith best regards... |
|
Follow us on