5/11/2010 1:54 PM | |
Joined: 8/31/2005 Last visit: 8/8/2025 Posts: 2198 Rating:
|
Hello Erdem Sivri!
You should use the IM174. This is the simpliest way to connect hydraulic axis.
You need to enable the axis (MC-Power), maybe reset it (MC-Reset)and then you have to give a position command (e.g. MC_MoveRelative). You should use a cam to improve the positioning performance. Have a look on the Technology Template "Hydraulics Characteristic"
If possible you should use S7-Tech(nology). SCOUT is only tested with SIMOTION controllers. It should work with T-CPU, but this is not tested. S7-Tech is tested with the T-CPU. You may use synchonation command (MC_GearIn or MC_CamIn) to synchronize the pos. axis to the one with const. speed. Like it is done in the application exampel"Feeder" . If you need a more complexe relationship you may use the Technology Template "Move 3D" .
see 3) |
|
|
Follow us on