11/24/2009 5:54 PM | |
Joined: 8/31/2005 Last visit: 8/8/2025 Posts: 2198 Rating:
|
Hello, I suggest you take a closer look at a CPU 314 or better on a 315. I'm not shure, but I expect they are fast enough if there is not much else they have to do. If possible, you should use one of this innovated CPUs. ------------------------------ Please note the FM350-2 allowws max. 10 kHz per channel, with 2500 Puls/turn you can only go up to 4 turns per second or 240turns per minute. ----------------------------- Why you want to use MM440 and not a "smaler" one like MM430. ---------------------------- If you think about using PROFIBUS, you may use the 1COUNT module |
Last edited by: miami at: 11/24/2009 6:42 PM |
|
Follow us on