6/3/2010 12:21 PM | |
Joined: 2/6/2009 Last visit: 9/1/2025 Posts: 940 Rating:
|
DearSM, Mr.autom8'ssuggestion is correct and easy way to configure the R-System.I used the same method in my project with R-System and it works well. In that method you can access both the CPU by connecting your PC/Adapter to one of the CPU. and download.Because, if you download the backup of CPU 1 to CPU2 then you will get system Fault. The reason for system fault will be same address on the both CPU's.In such case Remove the Linking Cable between both the CPU's and download one by one to avoid unnecessary tension. |
_______________________________________________________________ |
|
6/3/2010 8:28 PM | |
Posts: 382 Rating:
|
Hello, I hope I understand your question. Since both your CPUs MPI ports are used for software redundancy, you can also download your program using the DP port. If you want to download the programfrom the MPI port, you can consider using profibus connector with PC/PG so that you can piggy-bag your programming cable on to the connector without removing. You can also download to next station by selectingdifferent MPI address. Hope this helps! with regards, how come AttachmentProfibus Connector.zip (472 Downloads) |
Follow us on