(0)| 1/21/2011 5:16 PM | |
|
Posts: 15 Rating:
|
Hmm I cant really work out what you are asking for but, have you tryed changing the block name?. |
| 1/26/2011 11:48 PM | |
|
Posts: 1690 Rating:
|
Hi oximat, in the german forum part i have publish the motovation to sort the block numbers and the how to: Motivations are an easier direct programming at the LOGO!-basic-modules, an easier documentation AND (i think the most importent reasen is:) the better using of the parameter assignment mode (from the RUN-mode and without STOP the LOGO!-program-execution !!!) from the LOGO!-basic-modules. The changeing of blockparameters is possible in that mode if we presume that the respective default parameter protection mode (”+”) has been maintained. This is a prerequisite for viewing and editing parameters in the parameter assignment mode! The problem inside this mode is, that the blocks are (only and fix) sorted by blocknumbers (not by blocknames or blocktypes...)! If an operator want to modifying parameters of blocks witch are build a functiongroup of the application he must search and scroll around the blocks by ther numbers - not a good solution i think... 0) Remember, you need only sorted blocknumbers and between the sorted blocks you can have other blocknumbers witch are NOT listed in the parameter modus (means: blocks with parameter protection mode: ”-”) 1) If only some blocks must de sorted AND the programm have more free blocks in relation of the number of sorted blocks: 2) If only some blocks must de sorted AND the programm have NO more free blocks in relation of the number of sorted blocks: 3) If the number of blocks you want to sort high(er), then you should build a NEW programm (I know, that is a lot of work): Perhaps helpful links: |
Follow us on