(2)| 3/25/2007 9:26 PM | |
|
Posts: 1690 Rating:
|
Hi dmg, it is possible to convert the output of a counter block into values. Look at the example in the small LOGO-Programm. The number of pulses must be translated into a multiplexer and then you use one or more analoge amplifier to convert the value of the conterin a value of phys. units. To set the number of decimalsto n (1 to 5) it is equal to dividide by 1/n. But remember that the maximum value is not so big as the counter can count !!!Do notforget to clear/reset the counter by the USER.If you wont additional to convert impulses per time to a phys. unit look my comments at the german forum under: 1) velocity in thediplay 2) strokes per minutes
AttachmentPulses_to_Units.zip (1252 Downloads) |
| 3/25/2007 9:49 PM | |
|
Posts: 12 Rating:
|
Dear Betel, Many thanks for the elegant solution! Best regards, Dimitri |
Follow us on