9/20/2013 11:22 AM | |
Joined: 2/7/2013 Last visit: 10/6/2024 Posts: 21 Rating:
|
Hi, I am trying to configure a D425 (idevice) to a s7-1200 controller (IO controller). Here's what I did: 1.set up HW config in simotion scout 2.Export GSD file in Simotion scout 3. Import GSD file in TIA 4. Set up HW config in TIA But when I try to download to the s7-1200, It gives me an error which doesn't explain much, {Loading the hardware configuration failed (0020 0 2 0)} and When I download to the d425, there is a blinking red light on PN. I am not using CBE30 on my hardware, but I am using a standard ethernet hub. Will this still work? I know there has been several issues similar to this: /tf/WW/en/Posts/91961 /tf/WW/en/Posts/87339 But there hasn't been a solution yet, so any help is greatly appreciated. Attached are the screenshots for my setup AttachmentHwConfigCol.pdf (592 Downloads) |
Follow us on