9/27/2019 6:47 AM | |
Joined: 9/18/2015 Last visit: 11/29/2024 Posts: 47 Rating:
|
I export the GSD file in step7, then import into tia15. connect with cpu1214C, But can't connect. if it's possible? |
9/27/2019 12:56 PM | |
Joined: 4/3/2008 Last visit: 1/24/2025 Posts: 388 Rating:
|
If you have Simotion and PLC in the same project just mark the radio button and choose the IO controller in the drop-down menu If you need to latch a Step7-Scout component with a TIA Portal project 1200 you just have to watch out the following video link: pigroplc |
Last edited by: The Helping Hand at: 09/27/2019 13:32:02Embedded video. |
|
10/6/2019 6:19 AM | |
Joined: 9/18/2015 Last visit: 11/29/2024 Posts: 47 Rating:
|
Thanks. attached the detail error. Maybe must select the option"Force IEC V2.2 LLDP mode" ? |
10/6/2019 6:20 AM | |
Joined: 9/18/2015 Last visit: 11/29/2024 Posts: 47 Rating:
|
D425 hardware config |
Follow us on