9/19/2014 4:41 AM | |
Joined: 12/12/2011 Last visit: 7/23/2025 Posts: 69 Rating:
|
Dear Expert, i using C240 control (2CU) S120 CU320DP (attached file). One CU320 (crank1,2, Chain1,2). another CU320 (hoist,tilt,travel). when do commisioning i can control (crank1,2, chain 1,2), but i can not control CU320 (hoist,tilt,travel) from C240 program Scout. Please take a look attached file and help me. I realy rush onsite commisioing now. Much THANK!
AttachmentADVICE.zip (565 Downloads) |
Last edited by: Min_Moderator at: 9/19/2014 10:51 AMNew subject after splitting from /tf/WW/en/Posts/114519#top |
|
9/19/2014 5:37 AM | |
Joined: 12/12/2011 Last visit: 7/23/2025 Posts: 69 Rating:
|
Dear ChristophD, After actived Equidistans bus cycle on HW config follow YOU. then download Program, have Fault all Drive about Start address Profibus (crank1 startaddressDP 320, Crank2 startaddressDP 352, Chain1 startaddressDP 364,...) i think have problem with value of Equidistans bus cycle. Can you help me fast solve with attached file (Program, picture). Much Appriciated!
AttachmentHWCommsioning.zip (539 Downloads) |
9/19/2014 6:49 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
Hello, the bus settings are not optimal. you should use 12 mbit instead of 1.5 . I have modifiy the settings , you sould download all 3 devices (C240+CU320). This fault 20005 Reason 80h means that there are diferences between the axis config and the drive config. for detail information take a look in the diagnosticbuffer. Regards Christoph
AttachmentHwsite.zip (531 Downloads) |
9/23/2014 7:28 AM | |
Joined: 12/12/2011 Last visit: 7/23/2025 Posts: 69 Rating:
|
Hi Expert, Cycle clock cleared (time 4ms). but i still can not RUN C240 by fault show attached file. Your Posted i don't change any thing then downloaded it have this problem. i am doing commisioning but have many problem about communication. i am so rush, please Can you can help me solved?Maybe Baurate for Profibus 12mbps so Hight? Thank You!
AttachmentHwsit_and_FaultProfibus.zip (518 Downloads) |
Last edited by: Min_Moderator at: 9/23/2014 10:41 AMInclude program to attachment |
|
9/23/2014 8:09 AM | |
Joined: 12/12/2011 Last visit: 7/23/2025 Posts: 69 Rating:
|
Hi Expert, this file saved as by Scout! Thank you!
AttachmentDevice Diagnostics.zip (553 Downloads) |
Follow us on