5/4/2022 6:47 PM | |
Joined: 7/2/2015 Last visit: 8/25/2025 Posts: 96 Rating:
|
Hello omery, 1. You should configure the correct rack with the hardware configuration and later paste it at the same hardware config. 2. You should load the H system configuration, you have the instructions at the following link. 3 You should configure the selector of the PLC in 0, if there is no mistakes this one should be the master. Perhaps could be useful for you the following examples: - Configuration Examples for S7-400H with PROFINET - Realization of a Fault-Tolerant Tunnel Lighting System With S7-400H |
If this Information really helps, you could use the Rate function |
|
Follow us on