2/9/2023 7:21 AM | |
Joined: 4/28/2015 Last visit: 8/11/2025 Posts: 67 Rating:
|
Hello All I have been using CPU314C-2DP in our machine, CPUI counter module is being used for encoder feedback. The problem I am observing is that when speed is less than 600 rpm it is not showing speed feedback. above 600 rpm it is perfectly working !! I have confirmed encoder and cable and everything else is okay. Is it limitation of counter module ? SFB48 is being used for evaluation. I can see in program that MEAS_VAL parameter when above approximate 10000 is okay, but when lower than this , it shows zero. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/09/2023 13:40:49New subject after splitting There is only one end of Knowledge, The beginning. |
|
2/14/2023 6:43 AM | |
Joined: 4/28/2015 Last visit: 8/11/2025 Posts: 67 Rating:
|
no replies ! I hope I am able to explain my question !! |
There is only one end of Knowledge, The beginning. |
|
Follow us on