12/29/2021 7:54 AM | |
Joined: 2/2/2018 Last visit: 10/18/2022 Posts: 8 Rating:
|
hi. My name is TW. have a Question about CPU S7-416-2DP. 5days ago, we was shutdown main power for welding and yesterday main power on. and cpu diagnostic led (EXTF and BUSF 2F) is ON. checking hardware configuration online mode -> all die. was tried Profibus DP Line check and change Connector and DP address.....etc.. but ..Interface Module is die....TT so, CPU DP Port Change X2 -> X1 and Change Hardware Configuration. After Download, Interface module Connection!!!! but cpu diagnostic led (EXTF and BUSF 2F) is ON. i dont understand. why EXTF and BUSF 2F is ON? perhaps, CPU DP Port Self-Diagnostic and Shout? attached Diagnostic.txt Please help me.. Thanks. AttachmentDiagnose1.txt (726 Downloads) |
12/29/2021 8:10 AM | |
Joined: 7/9/2015 Last visit: 8/29/2025 Posts: 4443 Rating:
|
Hi, I checked diagnostic buffer and found Event 12 of 120: Event ID 16# 530D and Event ID 16# 5961 The reason could be the SDB. Please check this FAQ - pherhaps it will work: Why won't the IM and/or the CP with a CPU S7-400 go into RUN mode when the event ID 530D appears in the diagnostics buffer?Regards, Towome |
|
|
This contribution was helpful to
1 thankful Users |
12/30/2021 8:22 AM | |
Joined: 3/4/2019 Last visit: 2/16/2024 Posts: 18 Rating:
|
hi, the first check may be any device may power off or remove communication. so check all devices. |
Follow us on