1/6/2018 4:58 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35965 Rating:
|
In the german-speaking forum, the user Sierra83 has written a nice little software, which used an EXE file to set flags or bits in the VM area. This can be done as a pulse with adjustable length in milliseconds or as a continuous signal (also changing (toggle)). At this point, I would like to sincerely thank User Sierra83 for the program. AttachmentLogo_Updater.zip (372 Downloads) |
This contribution was helpful to
2 thankful Users |
Follow us on