10/10/2024 4:21 AM | |
Joined: 10/9/2024 Last visit: 6/13/2025 Posts: 12 Rating:
|
These are files that should be original to the machine, I don't understand Siemens' naming logic, but from what I observed, the files do not have headers that start with "%", the file named PCL I believe is what you call PCP, I didn't identify what L888 would be or the other so-called subprogramsX Attachmentparmetrosdafamupmcx700.zip (323 Downloads) |
10/10/2024 4:30 AM | |
Joined: 10/9/2024 Last visit: 6/13/2025 Posts: 12 Rating:
|
These are files that are from a machine from the same manufacturer said by the seller to be identical to the X700 only with larger axes, model x1000. I think there is some accessory that would be different, because looking at the original PCA file of the X700, which is the machine I am analyzing, the file in Portuguese shows an alarm from the chip conveyor that the machine has attached, already in the PCA file of the x1000 which is loaded into memory in English does not have the chip alarm code. I didn't try to load the x700 files again because I don't know if they are in good condition and it could make the machine's situation even worse, since the purchase agreement has not yet been finalized.
Attachmentparmetrosdafamupmcx1000comcomandosiemens810ga3.zip (326 Downloads) |
10/16/2024 2:44 AM | |
Joined: 10/9/2024 Last visit: 6/13/2025 Posts: 12 Rating:
|
let's go. I think now with the information we can continue. thank you. very much |
10/22/2024 1:49 AM | |
Joined: 10/9/2024 Last visit: 6/13/2025 Posts: 12 Rating:
|
Alarm=8 Message from nc = ord 1, wrong axis / spindle assign. |
Follow us on