2/16/2018 1:23 PM | |
Joined: 7/30/2012 Last visit: 7/23/2025 Posts: 335 Rating:
|
Hello I'm using Fb Cam Create In Simotion D425 If I Create cam manually (enter values in master and slave table in cam) its works fine master slave 0 0 190 0 260 10 If use this cam means slave axis rotate 10 degrees for mater 190 to 260 degrees sometimes i need to change this values so i'm using FB cam create but its not working for me axis rotate more than one rotation ( I’m seeing practically)but actual values saying only 10 degrees Note: master is a external Encoder and slave is a real axis for both have enabled modulo length as 360 in cam settings master evaluation is absolute and slave is relative finally I need to achieve result using FB cam create ....can anyone Terkel me how to create profiles and other thing for above values refer attachments AttachmentFBCam.zip (354 Downloads) |
Last edited by: @KB@ at: 2/16/2018 2:23:17 PMLast edited by: @KB@ at: 2/16/2018 2:28:48 PM |
|
2/18/2018 5:41 PM | |
Joined: 7/30/2012 Last visit: 7/23/2025 Posts: 335 Rating:
|
Hello !!! Any idea ??? |
Follow us on