1/23/2024 1:08 PM | |
Joined: 4/28/2015 Last visit: 2/21/2025 Posts: 3 Rating:
|
Hello I have a control unit CU230P-2DP( version 4.07.sp13.hf 2 )who is controlling a drive G120 PM330 (type 6SL331-1PE37-4AA0) 400kW. and working in DDC control I've done the motor ID (R3925.0 R3925.2 en R3925.3 are "1") did the copy ram to rom en saved the parmeters When i now turn off the power of the drive en switch on again the drive start for about 6 seconds with a Motor ID (R2 = 14) and then he takes over the setpoint I also tried with P1900 = 12, and the result is the same; Drive start up with Motor ID AttachmentSk27.zip (318 Downloads) |
1/26/2024 9:57 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject PM330 starting every time with a small Motor ID( approx. 6 sec) is published within the conference SINAMICS G. Jen_Moderator |
Follow us on