2/12/2017 10:25 PM | |
Joined: 8/25/2014 Last visit: 5/12/2025 Posts: 135 Rating:
|
Hello all. I have a KTP 300 basic panel that is connected to a LOGO8, that controls a mixing process. I've made 4 customizable programs for the users so that they can enter 4 parameters of the mixing process. I can’t user recipes because the interface for the recipes is too complicated to manage on this panel and the end user wanted a simpler way to enter and edit the parameters. The problem with my solution is that when there is a power cycle all the parameters are erased, because I don’t use tle LOGO’s retentive memory. So this is how the parameters are addresed: Parameter 1 - vw100 How can I make these addressees retentive in the LOGO memory, or alternately which addresses do I use so that the parameters will be saved to the LOGO memory Cheers A ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/13/2017 2:41:12 PMNew subject after splitting |
|
Follow us on