2/9/2022 8:32 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi vinayakparab81292, Unfortunately, i do not think there is a clear answer. Even if the system is not running continuously, there is not a clear answer, as the puffer time depends on the hardware built and must be calculated individually. In general, it is stated to change the battery "at the latest after one year". When should you replace the back-up battery on your S7 300/400 controller?How great is the power requirement (from the backup battery) of the modules to be backed up at "Power Off" and what is the relationship between the backup current and the length of the backup time?
regards sancruz |
Feedback appreciated, please rate |
|
Follow us on