3/22/2010 8:04 AM | |
Joined: 9/29/2005 Last visit: 7/16/2025 Posts: 313 Rating:
|
Hi, i found this info in the internet: Our advise in this case is to set up environment from the very beginning, remembering, when use eclipse, to set up the eclipse server delay by: Window -> Preferences -> J2ME -> "Debug Server Delay (ms) to 25000ms. Regarding the configuration file – statement is that user should only comment and uncomment particular lines in it - and change only the values of parameter. It’s recommended not to change the syntax of the file. If user will have the problem with debug, even after changing the delay, then should submit more detailed info describing where is the problem (e.g. error messages). In overall: - eclipse should work fine after set up delay, if needed there is step-by-step document prepared for eclipse debugging. Far I know it’s not confidential. Think we can upload this one to the forum (please find it attached) - may be also related - far I remember there is problem with debugging on USB on WinSP3 - it is fixed on newest (not released yet) software Furthermore have a look to the attached documentation which will maybe help you in the process of debugging.regards Lifrasil AttachmentJava Debugging step by step.pdf (628 Downloads) |
Follow us on