4/3/2019 10:34 AM | |
Posts: 5 Rating:
|
HI, Can anyone help me with this communication error? I have made 2 sample program for S7-200 Smart CPU ST60 in MicroWIN Smart v2.3 for TCP communication using OUC library TCP_Connect, TCP_Send, TCP_Rcv, TCP_Disconect. This sample program is given in the Help of MicroWIN Smart v2.3. I get two error while downloading. Error-1 When I click download, It open communication window in that when I select the plc and click ok then shows error - An error occurred while receiving data from PLC Error-2 When communication is okay and I try to download this program I get an Error - An compile error occurred, check non-fatal error. After Closing this when recompiling the program I get Error - The instruction is not supported by CPU type Selected. I am attaching my program along with error images Thanks and Regards ------------------------------------------------------------------------------------------ AttachmentERROR.zip (488 Downloads) |
Last edited by: Jen_Moderator at: 4/3/2019 12:43:49 PMNew subject after splitting |
|
Follow us on