6/18/2013 8:38 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
Hello, no this CF-Card is not usabel with the SIMOTION D425-2. You must update the bootloader and the FW on the card. FW Version must be V4.3.1.x (D4x5_2_V43SP1HF12_S120_V45HF14.zip ). http://support.automation.siemens.com/WW/view/en/31045047 The bootloader is installed with scout and can be updated on the CF Card via SIMOTION Scout. Regards Christoph |
Last edited by: ChristophD at: 6/18/2013 8:42 AM |
|
This contribution was helpful to
1 thankful Users |
6/18/2013 9:16 AM | |
Posts: 205 Rating:
|
Hello ChristophD, thanks for your replay.. i have downloaed latest firmware ..i want to know about bootloader file.. i am attaching screenshot of bootloader file selection for D425-2DP controller.... the bootloader file i have selected,Is it true?????????? AttachmentAttachment.zip (379 Downloads) |
6/18/2013 9:17 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
Hello, yes this is the right bootloader. Regards Christoph |
6/18/2013 9:26 AM | |
Posts: 116 Rating:
|
Hi, by the way: see http://support.automation.siemens.com/WW/view/en/18857317 chapter 2.5 --> there you'll find detailled compatibility information. Regards Jerry |
6/18/2013 12:29 PM | |
Posts: 205 Rating:
|
Hello, Thanks for your help..... |
6/26/2013 7:33 AM | |
Posts: 205 Rating:
|
hi jerry, thanks for this link... |
Follow us on