12/30/2023 1:37 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, There are two ways to migrate a project: Which one did you do? With new functions means you are updating the basic library and AP library to the latest versions, possibly migrating a classic library V7.1 SP4 to APL. You can however use the same library in a new PCS7 version (without new functions). Please make sure the manual is followed to the detail. If you migrate with new functions, you need to upgrade in steps. Those steps are explained in the manual: Update with new functions. One other aspect is making sure you have only one version of driver blocks in your AS project. Please check if there are older versions in your Blocks folder. Another aspect is APL and Basic library mismatch that can occur. Make sure the readme notes are check and check them for compatibility. Can you tell us how you did the migration with some screenshots like Installed software |
Last edited by: Jen_Moderator at: 01/02/2024 08:39:03Links optimized. If I could help you, you can use the RATE button. Thank you. |
|
1/26/2024 12:57 PM | |
Joined: 8/1/2022 Last visit: 7/28/2025 Posts: 8 Rating:
|
thank you for reply i just take project archive and then retrive in new version of PCS 7 V9.0 . |
Follow us on