2/16/2012 8:33 PM | |
Posts: 4 Rating:
|
Hello, Trying to create a simple step program with delaytime between every input in random order. Got it working for2 random inputs now want to go to 6 inputs so added more into it. But now i got stuck !!! For 2 randoms inputs (1&4) it works fine and then push another 2 inputs (6&2) after that works also. But when i want to go to 3 inputs at1 time (or all 6 inputs) it stops and doesn't go further. Anyone got a suggestion to get me further ?? Thxs AttachmentCOMPLEX FINAL.zip (387 Downloads) |
2/24/2012 4:14 PM | |
Posts: 378 Rating:
|
Hello, I couldn't open your file (I have old version of logosoft comfort) but I attached here my sample program. Here is my steps of writting: 1. I use random time generator for random values beetween 00:00 to 02:40 seconds 2. I use pulse generator on time 00:20 and off time 00:20 (make shure your scan time is less than 00:20 or inclrease the values acordingly). 3. From above if the randomly generated value is 02:40 there will be 00:20 X 6 ON pulse and 00:20 X 6 OFF pulses. 4. I use counter to count this pulses to get in to numeric values 5. Now the randomly generated time values (00:00 to 02:40 ) are converted to random numeric values (1 to 6). 6. By using counters I compaired to randomly generated numeric values to 1, 2, ...,6 then I asscociated to Inputs I1, I2, I3...., I6 7. For simulation purpose I use inverted inputs I1, I2,....,I6 and output to Q1,Q2,....Q6. I hope it will be helpfull for you and you can make it further short, By the way what is your application area for this program? It's odd and interesting for me! AttachmentMyComplex.zip (393 Downloads) |
Follow us on