11/13/2019 3:44 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello Kiiza; Sorry, the TD200 and TD200C test diaplays were designed only for the S7-200 family and are being removed from production at this time, since they were to be programmed with Microwin and the S7-200 line is discontinued. Same thing is now happening with the newer TD400C, a 4-line display. To connect to a S7-1200, you need a unit with a Profinet (or eventually a Profibus optional port), and Siemens has decided to produce only graphics panels in that design. See this presentation brochure for a listing of available units: https://c4b.gss.siemens.com/resources/images/articles/dffa-b10135-03-7600.pdf The smallest panel that is designed to connect with a S7-1200 (it has a Profinet port, and is to be programmed with WinCC Basic (from version 11)) is the KP300 Basic Mono PN, 6AV6647-0AH11-3AX0,for which you can open the technical data here: Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
11/20/2019 7:12 AM | |
Joined: 11/17/2014 Last visit: 8/28/2023 Posts: 184 Rating:
|
Thank you very much Daniel, This is very helpful. |
Follow us on