3/12/2019 9:00 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, wrong FW in the CU320! You have in the project a CU320 V2.6.2 v´created and in the Target the FW Version V2.3 is active. Upgrade the FW in the Target CU320 to V2.6.2 to connect it. SINAMICS S120 Firmware Version 2.6 SP2 HF19 or delete the V2.6.2 CU320 in HWConfig and create a V2.3 device. Regards Christoph |
Last edited by: ChristophD at: 3/12/2019 9:02:53 AM |
|
This contribution was helpful to
1 thankful Users |
3/12/2019 4:03 PM | |
Posts: 10 Rating:
|
Hello christoph, I will check the messages tommorow. And also try to change hw offline. Kind regards |
Follow us on