8/19/2020 9:26 AM | |
Posts: 4 Rating:
|
Hello, through manual diving and the example program provided by siemens (attached as zip) i've gotten a decent understanding of how the card reader works. However, i haven't been able to find any information on the telegrams beyond the what i can deduct from the example code. Below is the addressing used to write a colour of the LED in the card reader. //Request "syscmd_set_port" telegram #statWriteData[0] := 16#0C; #statWriteData[2] := 16#07; #statWriteData[3] := 16#02; #statWriteData[6] := 16#01; //ColorLED;0x01 (green), 0x02 (red) Where can i find information explaining that the addressing above is used to access the LED and more importantly the addressing of other telegrams not used in the example program (specifically the one used to rewrite the UID of cards)? -Nivagn Attachment109770535_RFID_RF1070R_RS232_RF170C_PROJ_TIAP15_1_V1_0.zip (939 Downloads) |
8/20/2020 8:36 AM | |
Posts: 4 Rating:
|
I found the answer in BA_RF170C_76_en-US which i have attached if anyone is interested in the information.
AttachmentBA_RF170C_76_en-US.pdf (1002 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on