11/9/2018 10:22 AM | |
Joined: 3/2/2007 Last visit: 9/9/2025 Posts: 990 Rating:
|
Kindly, we need to use a Simotion D410-2 as master for many S120 axis. Which hardware should we use? Which control units? And which memory cards? Thank you 6AU1410-2AD00-0AA0 , SIMOTION Drive-based Control Unit D410-2 DP/PN; programmable single-axis motion controller with multi-axis option; interfaces: 5 DI, 8 DI/DO, 3 F-DI, 1 F-DO, 1 AI, 1 encoder, 1 DRIVE-CLiQ, 1 PROFIBUS, 2 PROFINET ports, 1 ethernet Note: requires at least SCOUT/firmware V4.3 SP1 HF3 6AU1820-0AA41-0AB0 , SIMOTION TECHNOLOGY OPTION MULTIAXES PACKAGE SINGLE LICENSE ON PAPER FOR ONE D410-2 (is this package required?) |
... thank you ... |
|
Follow us on