6/25/2011 7:33 AM | |
Posts: 80 Rating:
|
Dear Friends, I was trying to integrate Sinamics DCM (6RA80) in Simotion and found following result. - I was not able to configure DCM through sinamics integrated - Even DCM not showing in "Insert Single Drive Unit" - Installed SSP for DCM. - Now i can configured DCM throgh "Inser Single Drive Unit". - The view of my projet is as attached snap. I am having following questions 1) can we integrate DCM throgh its drive-cliq port with simotion? 2) Does DCM having Profibus port bydefault or any option card needed? 2) Has anybody done Rotary cutter application using Simotion-DCM?Because we are going to use DCM for rotary cutter application using Simotion and had never used DCM till so far. Rgds Ashish Attachmentdcm.pdf (634 Downloads) |
6/25/2011 4:20 PM | |
Posts: 344 Rating:
|
1. Sinamics DC Master drives has it's own control unit. It does not need to and cannot be connected to DriveCliQ ports of Sinamics_Integrated. It is connected to Simtion with Profibus or Profinet. 2. Profibus comes standard, Profinet is optional. 3.Simotion Rotary Knife application. is available The example is using S120 drives, but it can be adapted to DCM as well. |
5/4/2012 10:01 AM | |
Posts: 9 Rating:
|
Hi I am also trying to find idea about Rotary cutter application for past 2 days Its very useful to me thank you. |
5/21/2012 12:42 PM | |
Posts: 344 Rating:
|
Simotion Rotary Knife application |
Follow us on