3/10/2016 9:31 AM | |
Joined: 3/14/2008 Last visit: 9/16/2025 Posts: 2216 Rating:
|
Hello Tom, Did you update the PCS7 version? Is your project created in a different version and your trying to migrate? You have to migrate from version to version. You cannot go from v6.1 to 8.0 for example.. Please follow the manual: "Software update with utilization of new functions" depending on your PCS7 current version. |
If I could help you, you can use the RATE button. Thank you. |
|
3/10/2016 2:58 PM | |
Joined: 3/14/2008 Last visit: 9/16/2025 Posts: 2216 Rating:
|
Well, When the blocks are updated to the new version, you have to do a full compile of the charts. You can delete the @charts, only if you have F-blocks, which are not updated to the new technology, then they shouldn't be deleted. To which version did you update. I believe you have to update from v6.1 to 7.1 SP3 or SP4. And then to 8.x. Not a update from v6.1 to 7.1 SP1 or SP2.
|
Last edited by: Oreca at: 3/10/2016 3:02:49 PMIf I could help you, you can use the RATE button. Thank you. |
|
3/11/2016 7:12 AM | |
Joined: 3/14/2008 Last visit: 9/16/2025 Posts: 2216 Rating:
|
Morning!, Are there any blocks which originate from a PCS7 add-on library, like Simocode or something, which now doesn't work with your new version? |
If I could help you, you can use the RATE button. Thank you. |
|
3/11/2016 3:09 PM | |
Joined: 3/14/2008 Last visit: 9/16/2025 Posts: 2216 Rating:
|
Hi Tomact, Hmm very strange.. These xml's files are standard install files. Maybe you can track down the date of change of the xml file to check if it was changed recently. The location: C:\Program Files (x86)\SIEMENS\STEP7\S7DATA\driver\action\08010000 lists all xml files. --> al_cpu.xml |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
8/27/2018 3:04 PM | |
Joined: 10/13/2016 Last visit: 5/24/2023 Posts: 1 Rating:
|
Thaks Man! problem solved! |
Follow us on