2/4/2020 7:14 AM | |
Posts: 137 Rating:
|
ByTheWay i am Trying ...This and not working I tryed to build like in Simotion a Struct and define Int and array then i tryed to Overlap not working .. when i define 2 variable in Static like INT and array byte it works ... so that's the Soultion ? i dont need Struct OVERLAP ... just 2 variable in STATIC in my FB and with AT ... and it's work same like in SIMOTION true ? Actually here come to my mind another Question ... what the diffrent if i define in my FB interface in Static a Struct include 2 variable (Int) and ( array of 2bytes ) or i just define 2 variable without Struct ( Int ) and ( array of 2 bytes ) . like in Attachment ... i could AT ( Overlaping ) just in case without Struct ... or there is a way to do overlapping with Struct ? and in my case is it True i give the AT to the second variable ? if i want to be exactlly like my example in SIMOTION
|
Last edited by: Inv0ker at: 02/04/2020 07:19:10Last edited by: Inv0ker at: 02/04/2020 07:32:15Last edited by: Inv0ker at: 02/04/2020 07:33:51Last edited by: Inv0ker at: 02/04/2020 07:36:16 |
|
2/4/2020 8:51 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi together, How do you program the overlapping of tags with the keyword "AT" in the STEP 7 (TIA Portal)? It should explain what AT is and how to use it. hope this helps, regards |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
Follow us on