5/3/2011 12:05 PM | |
Joined: 9/23/2005 Last visit: 9/3/2025 Posts: 4416 Rating:
|
Hi, Some notes: 1 - "Will V11 allow me to compile as 10.5 and download to 1.x firmware PLCs?" Note: STEP 7 Basic V11 program S7-1200 CPU with firmware V1.0, and V2.0. So, you don't need to change de CPU firmware to work with STEP 7 Basic V11. 2 - I have a project which will be starting very soon. What timeframe should the SUS update be expected now that it officially released? If I upgrade, will I lose the ability to log on and communicate with the existing projects? Note: In readme.pfd file for STEP 7 V11 (http://support.automation.siemens.com/WW/view/de/49639088) are points to be observed if you intend to convert the program. In special, I copy this part of page 27: "To monitor and test a program converted from STEP 7 V10.5, you have to first compile and load with STEP 7 V11.0." If I right understand, you don't have yet the V11, but it comes soon to you. My suggestion is to take a look at the open FAQ, and see what you will need to do if you start with 10.5 and migrate "on the fly" to V11. Thereare many improvements in V11, so make sense to use it. |
Denilson Pegaia |
|
Follow us on