4/7/2025 9:03 AM | |
Joined: 3/22/2025 Last visit: 4/11/2025 Posts: 10 Rating:
|
Hello Logo community,
I came back to you with the following problem: When I try to connect to a logo 8.3 I can detect the ip address but when I try to switch it to stop mode or upload a program, it gives me the following error: “Logo 8.3 CA is not trusted. The remote device is not accessible.” I have installed the root certificates from the “res” file that I found under the path where logo software is installed but still is not working and I encounter the same error. I found this topic on forum and followed it but maybe I`m doing something wrong: https://support.industry.siemens.com/forum/ro/en/posts/download-error-in-logo8/317113 Some more details that may be relevant: - I run Logo soft comfort version 8.4 installed on a USB 3.0 flash drive (because my laptop is old and I read on forum that in case I won`t be able to access the computer I will loose my license). The “res” file mentioned above is installed/present on usb drive. - Actually I have 5 pcs of 8.2 FS4 controllers that I could connect to them and modify as intended an only one 8.3 controller on which I can`t connect. |
4/7/2025 11:16 AM | |
Joined: 12/18/2014 Last visit: 9/2/2025 Posts: 35913 Rating:
|
Take a look at attached PDF.
AttachmentLOGO! 8 manual 0BA8 2024_08 xxxx8-0BA2 pages 317-332.pdf (312 Downloads) |
4/9/2025 4:47 PM | |
Joined: 3/22/2025 Last visit: 4/11/2025 Posts: 10 Rating:
|
In the attached snapshot is the error I get |
4/9/2025 5:15 PM | |
Joined: 12/18/2014 Last visit: 9/2/2025 Posts: 35913 Rating:
|
Start a Support Request. |
This contribution was helpful to
1 thankful Users |
Follow us on