6/25/2010 7:27 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
Hi Projjwalu You can have CP5512 card which will be usefull in your case. You can configure5 it as profibus or MPI protocol. I have CP5512 card for service call and i find it very usefull. Please note: That the CP5512 card is PCI / MCI slot card, See attachment for more details. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=6GK15512AA00&caller=view |
Jazz |
|
6/25/2010 7:40 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
For download or booting (filling in the case of a missing or damaged operating system) to the OP77A you need either 6ES7 901-3CB30-0XA0, either 6ES7 901-3DB30-0XA0. Note! The RS232/PPI Multi Master cable (with 8 DIP switches) can be used if DIP switch number 5 is set to PPI/freeport ("0"). The cable must be dead for it to accept the change. Note: The USB/PPI Multi Master cable (Order Number 6ES7 901-3DB30-0XA0) E-Stand 05 can be used for downloading since WinCC flexible 2005 SP1! For process coupling, update operating system, project use 6ES7 901-0BF00-0AA0 Backup is only possible using Prosave.(How do you backup/restore with a Windows-based panel? ). Best regards, Hristo Mihalev |
6/27/2010 8:19 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread S7 USB PC Adapter. Best regards O_Moderator |
Follow us on