(0)| 2/10/2011 11:16 PM | |
|
Joined: 11/10/2010 Last visit: 11/2/2025 Posts: 24 Rating:
|
Hi all, i have problem with step 5 which refuses to switch in online mode.I have proceeded to reinstall step 5 but it is the same situation.The message is " time out" or alarm 0334 with all the ports.I have a PG P4 with ibox.The serial port Db9 on ibox works.Please help.
Splitted from s5 . |
Last edited by: O_Moderator at: 2/11/2011 8:29 AMnew subject after splitting |
|
| 2/11/2011 7:43 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Perhaps will helps you - System message no. 0334" when attempting to go online with STEP 5 V7.2 in Windows XP Best regards, Hristo Mihalev |
| 2/12/2011 1:07 PM | |
|
Posts: 8946 Rating:
|
Appear same problem with an other CPU? Cable is OK? Setting (TTY, COM1) is OK? Which CPU? |
| 2/12/2011 7:24 PM | |
|
Joined: 11/10/2010 Last visit: 11/2/2025 Posts: 24 Rating:
|
Hi, the cable is ok too! |
| 2/14/2011 11:30 AM | |
|
Posts: 1064 Rating:
|
Check and make sure that your interface is set to as511 and parameter is com1 standard |
Follow us on