11/18/2014 6:41 AM | |
Posts: 5225 Rating:
|
Dear Forum Friends, The next update for TIA Portal V13 is available at [LINK]. Update 5 has been pulled back as there were some issues with the update. For those of us that has Update 5 installed, it is recommended to update to Update 6. Please let our community know if you have feedback on Update 6 that is worth knowing. (Thanks) Greetings. w NOTE (2015.11.18) This post was a notification of TIA Portal V13 SP0 Update 6. The current version is TIA Portal V13 SP1 Update 5. The updates for TIA V13.1 can be found {here}. |
Last edited by: William_B at: 11/18/2015 10:07:27 AMAdd note. |
|
This contribution was helpful to
3 thankful Users |
11/20/2014 1:53 PM | |
Joined: 6/30/2008 Last visit: 7/26/2022 Posts: 12 Rating:
|
Until now, After working 5 min using upd6... I've gor the first crash!! almost a record |
11/19/2015 9:11 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by AutoGen_756614 is split to a separate thread with the subject Can't install UP 6. Best regards |
11/19/2015 9:12 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4760 Rating:
|
New question published by Toombs is split to a separate thread with the subject Update 5 for SP1 more stable then Update 4?. Best regards |
Follow us on