4/28/2022 3:06 PM | |
Joined: 5/16/2016 Last visit: 2/22/2023 Posts: 53 Rating:
|
After the SMC20 replacement nothing has changed. 001: the drive commissioning ("CHANGE") with the SMC20 (2th encoder). The first one is drivecliq motor encoder. 002: encoder successful identified (resolution 20000 nm - correct) 003: same encoder info from another page 004: some parameters about the encoder (assigned to W axis) 005: others parameters 006: the axis assigment AX6 (SP1) is the main spindle. I've followed the same method to configure the rotary encoder (the working one). I hope that help you to help me. Thank you, AttachmentEncoderErr25000.zip (630 Downloads) |
Follow us on