5/24/2023 4:58 PM | |
Joined: 5/6/2010 Last visit: 8/31/2025 Posts: 2029 Rating:
|
Hello, you can do this in a lot different ways. One solution for a 1200/1500 is that you use a frequency generator, e.g. LGF_frequency from the Library of general functions (LGF) for SIMATIC STEP 7 (TIA Portal) and SIMATIC S7-1200 / S7-1500 You parameterize them so that you have a signal which change every 200 seconds. Then you can switch with a logic that when the output signal of the generator is FALSE Fan 1 to 4 is running and when the signal is TRUE, the other fans are running. Also work it with a clock generator with 2 timers. There are so much more solutions for this challenge. This solution is only one suggestion. Hope this is a little bit helpful. regards |
5/30/2023 6:56 AM | |
Posts: 3 Rating:
|
Thank you very much ! |
Follow us on