10/20/2020 3:20 PM | |
Posts: 38 Rating:
|
Hi, that's indeed my plan ! Any advice ? |
10/22/2020 9:18 PM | |
Posts: 38 Rating:
|
Hello again, I have asked addtional information. This is what I have received so far. Would this be enough ? Link to API documentation : I still need to learn how to program the IOT20XX like I did with the LOGO. Goal is to use the data from the cloud as input to the LOGO that would then open or close a switch or generate a 0-10V value. |
10/26/2020 9:41 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, for the mentioned swagger there are some node-red nodes. You can check them out and see if the provide the functionality you need. If yes you can install them and use them with node-red. I haven't worked with swagger so far, so I think I can't really support here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on