6/29/2010 3:12 PM | |
Posts: 3 Rating:
|
Hi everybody, I've bought a Flowmeter from Bronkhorst with a Profibus-DP interface. Unfortunately, I don't manage to make it work. I want tolink itto a computer with a CP5613_A2 inside. PG/PC is set to CP5613_5614(PROFIBUS) and the device is recognized with the diagnostic test (white box at address 10 (and white checked box at address 0)). However, when I launched LifeList, it said that theslave at address 10 is not ready for data exchangeand that it should be reparametrized. I've find a documentation wich shows how to configure the device with Sycon (http://www.bronkhorst.com/files/downloads/manuals_english/917025manual_profibusdp_interface.pdf ), but I only have Siemens software. I have never had such problem, and I'm not really used to Step7. I really need some help to understand what isn't working and how to fix it. Thanks! |
6/29/2010 5:33 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello Albenejean; OK, my mistake. I didn't realize that you had no DP master program (PLC, WinCC) controlling the CP 5613 interface and acting as a Profibus master to your slave. So I suggest you look at the following manual, "SIMATIC NET DP Base Programming Interface for CP 5613/CP 5614", that you can download here: http://support.automation.siemens.com/WW/view/en/1653531 It will guide you in programming a master interface that will then be able to access your slave and collect data. The C/Delphi interface blocks (dll file)should be on the Simatic Net CD that came with the CP 5613. The software for the CP 5613 is also OPC compliant, so you could develop your own program to access the master functions. Start with the FAQ chapter, it should clear many things up. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/29/2010 5:36 PM |
|
Follow us on