5/18/2020 7:17 PM | |
Joined: 10/10/2017 Last visit: 10/31/2024 Posts: 61 Rating:
|
Hi, I am trying to connect my PLC 1215 and D435 2 DP/PN Control unit which is part of back to back topology of Siemens drive. I want to do simple task like sending speed reference via Profinet. So far I have done this by using GSD files of the device to which I want to send the data (for example Danfoss FC 302 frequency converter, etc.), however I can not find GSD file for this CU unit. Can anybody help me with advice, please? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/19/2020 06:27:09New subject after splitting |
|
5/19/2020 12:45 PM | |
Joined: 10/10/2017 Last visit: 10/31/2024 Posts: 61 Rating:
|
Yes, there is a program that I programmed and uploaded in D435. |
5/19/2020 1:02 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
you mean you will create a project and download it to the simotion? which TIA Portal you use? |
Follow us on