2/19/2019 9:33 PM | |
Joined: 12/13/2015 Last visit: 5/7/2024 Posts: 22 Rating:
|
hi, i can t communicat with my tp177b with the adapter siemens, but when this ihm is in a profibus network it s ok and i can uploid the bakckup, wath i can do for upload the backup without the net network, just with a adapter mpi ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 2/20/2019 10:15:36 AMNew subject after splitting |
|
2/20/2019 10:56 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello, Please can you give the MLFB number of the adapter you use? Perhaps this link is helpful: Which connector cables are available for connecting to SIMATIC Panels? Best regards, Wizard |
2/21/2019 1:14 PM | |
Joined: 12/13/2015 Last visit: 5/7/2024 Posts: 22 Rating:
|
hi Mr WIZARD the number for my adapter is ( PC Adapter USB(6ES7 972-0CB20-0XA0)) when i m in the profibus network for the machine it s ok i can uplaod the back from the panel, i have no probleme, but when i went work in my office with this panel for uploid the backup without stope the machine , she can't communicat ni with profibus parametres ni with mpi... |
Last edited by: electrikman at: 2/21/2019 1:16:50 PM |
|
Follow us on