2/18/2011 9:41 AM | |
Posts: 63 Rating:
|
Hello, I'm trying to connect my PG to our MM430 drive. Unfortunately this is not possible. I use an BOP connectiing kit, which I bought at Siemens. When I place the BOP-link I see that the LED lights don't lit up both. Only the green (left) LED lis lit. I configured Starter to the USS portal, with busadres 0. When I want to connect to the drive it say's it can't connect (please see the attachment). When I search for any available drive it do say's it found one, with busadres 0. When I disconnect the cable it can;t find any drives. So I gues the connectingcable and BOP are ok. The thing is that I can;t select the drive an connect to it. The type of drive is ok (MM430) with the exact formware (v2.1). However it still don't want's to onnect to starter. Does anybody have any clue or tips ? Please see the attachment for screenshots. Regards, Remo Attachmentstarterconnect.zip (215 Downloads) |
2/18/2011 11:41 AM | |
Posts: 739 Rating:
|
Pls. see the following FAQ: http://support.automation.siemens.com/WW/view/en/20016155 http://support.automation.siemens.com/WW/view/en/31399077 |
2/18/2011 11:18 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, which version of Starter are you using, you need at least Starter 4.1.1.2 to correctly display and connect to this drive. please download the latest version of Starter herehttp://support.automation.siemens.com/WW/view/en/26233208 Regards, Graeme
|
Follow us on