4/8/2012 5:14 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, An MP277 is configured using the engineering tool WinCC Flexible. If the tool is installed on a programming running Step7, you can run integrated with Step7. This means that for instance you can place the HMI in your Step7 project where aso the CPUs are configured. Now open the MP277 object, WinCC Flexible opensand in the tab connections WinCC Flexible will normally add connections to your CPUs, and if not you can easily add them by browsing the project. WinCC Flexible "getting started" is here: http://support.automation.siemens.com/WW/view/en/18660846 |
Best regards |
|
4/8/2012 7:52 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, You need to configure two connection in WinCC Flex. Each connection will have corresponding CPU. If one of CPUs is turned off there is receiving data from the other CPU only. How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? best regards, Hristo Mihalev |
4/9/2012 8:41 AM | |
Posts: 22 Rating:
|
yes, this CPUs have different programs and control seperate equipment, but for have common alarm logging in HMI i need to have a simultaneose communication between both CPUs and HMI. I find a support document from siemens that tell how many simoltaneose active controller i can connect with my panel. address is: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=15363798&caller=view but how? thankyou for your attention. |
Last edited by: vahidpc at: 4/9/2012 8:43 AMLast edited by: vahidpc at: 4/9/2012 8:42 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on